Part Number: TMS320F28386D
when check the detail of this part GPREG2 Usage and MPOST Configuration.
I want to enable the MPOST. But I only have one F28386D board, I worried about below question.
The Z1-GPREG2 register is the OTP? And Z2-GPREG2 register is supercede zone for Z1-GPREG2 register.
Does that mean I only have two times for configurate the mode of Run MPOST?
(One time to configurate Z1-GPREG2, another time to configurate Z2-GPREG2)
0x0 = MPOST is run with PLL enabled for high speed (110 MHz).
0xC = MPOST is run with PLL enabled for medium speed (80 MHz).
0x3 = MPOST is run with PLL enabled for low speed (60 MHz).
0x9 = MPOST is run using INTOSC2 with PLL disabled (10 MHz).
Any other value = MPOST does not run.