Other Parts Discussed in Thread: TMDSCNCD28379D
Hi,
I am working on a 29379D system which is connected through SPI and Serial comm to a Sitara ARM processor running an OS. Is there any way to run an firmware upgrade to 28379D through the ARM processor? The objective is to be able to send the required file to the ARM processor from a PC and then pass it from the ARM processor to the 28379D for the firmware update.
I can see in the LaunchXL28379 Users Guide (Rev C) it is mentioned that the SCIA pins routed to the XDS are not valid SCI boot pins and that the LaunchPad is not capable of using Boot to SCI boot mode. Does this mean we cannot upload the firmware externally on the launchpad by any method? Is there any other method of doing this through the ARM processor. Any suggestions or direction to documentation that I can read would be really helpful.
Thank you,
Aditya