This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386D: Power-On Reset

Expert 2380 points
Part Number: TMS320F28386D


When I perform the Power-On Reset on my device.

I check the ResetCauseValue = SysCtl_getResetCause();

I got different ResetCauseValue as below.

1. When power off, then power on,  connect with  debug, the ResetCauseValue is 0x C0 00 00 00 

2. Do the same operation, power off, then power on, use the SCIA to send out the ResetCauseValue  is 40 00 00 02

This make me confused.  The second way's result shows that the Boot ROM did not clear the reset cause register (RESC)