Part Number: TMS320F280039C
Hello,
I've recently got the serial flash programmer functionality working for my device and have been testing it with different sized application programs and baud rates. The highest reliable baud rate I can use is 115200 bps.
If my understanding of updating flash is correct, I was wondering if it was possible to alter the flash kernel to have a larger RAM buffer to load the program into, resulting in more of the application being programmed into flash at a time and fewer writes to flash overall?
I saw that there were requirements for the size of the buffer. Specifically that the size must be a multiple of 64 bits and be divisible by 4.

I've tried setting the BUFFER_SIZE to 0x100, but the program stalls. Is there potentially something else that also needs to be changed whether in the kernel or on the PC/executable side? Or perhaps there's a reason the buffer was originally set to 0x80 and shouldn't be changed? This is the command prompt showing where it stalls (a have to control C to exit the program):


Thanks!
-Emma