This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Unable to program flash memory using XDS110 Debug Probe

Part Number: TMS320F28388D


Unable to program flash memory using XDS110 debug probe ,showing error connecting to target please find in the below capture

Even tried running controller in CCS workspace debug mode showed the same error as above unable to connected, tried power cycling the board aswell

these are the observation we have regarding the issue

1. Checked the power rails and voltage levels to the controller and all are in the required values

2. With existing application firmware already in flash memory of ti controller, we were able to access flash by erasing and writing on to the flash sector.

3. At the TMS pin it is showing 0V though it is pulled up with resistor 2.2K

The circuit for interfacing JTAG is as follows

The controller is TMS320F28388D and operated at clock frequency of 25MHz connected to X1 pin of the controller

Thanks 

Pranay