This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IQ numbering and normalizing into pu - F28335

Dear,

 

I am a bit confused with the numbering systems. The IQ numbering confuses me.

I am working on the implementation of a control strategy for a three-phase inverter for distributed generation purposes. I measure voltages and currents which I for voltage and current controller. I use the ADC to measure them but then the problem is presented.

With my previous (a freescale dsp) I did the following:

// get adc values

iA=getReg(ADCA_ADRSLT0);

// substract offset

IA=(int)iA-iA_off;

/*

Rescaling variables

 

@ 3.3V the following quantities are measuerd

va=407V ia=29.97A

vb=350V ib=30.36A

vc=364 V ic=30.70A

vdc,ond=466 V vdc,bov=464V

 

For phase voltage: reference Vref=364 V

For dc voltage reference: Vdcondref=466 V

For the current Iref=30.70 A

 

 

ia=mult(IA,27811)<<1; // multiply with 29.97/30.7*32768 en multiply with 2

ib=mult(IB,32406)<<1; // vermenigvuldigen met 30.36/30.7*32768 en dan maal 2

ic=IC<<1; // vermenigvuldigen met 2

 

va=VA<<1; // vermenigvuldigen met 2

vb=mult(VB,31506)<<1; // vermenigvuldigen met 350/407*32768 en dan maal 2

vc=VC<<1; // vermenigvuldigen met 364/407*32768 en dan maal 2

 

vdcond=mult(VDCOND,32627); //vermenigvuldigen met 464/466*32768

/* Current control */

ierra=iwa-ia;

// P controller

drat=mult(Ki,ierra)<<Ki_scale;

 

But when I try this with the F28335, it goes wrong. When I was searching this forum for an answer, I found an example on the PMSM sensorless example where the same steps are followed, namely:ADC Result, normalized into pu, adjust for offset, normalize to +/-1 pu, scale to 3.3V from 3V ADC input.

But there I see that the ADC Result is divided by 2^12. and then the offset is substracted. I find it very strange that the ADC result is divided by 2^12 which is the same at a bit shift by 12 bits to the right.. Therefore I am a bit confused. Can someone explain me how this division is justified? I must say that I am used working with a 16-bit processor and that the F28335 is 32-bit one.

Thanks in advance!

My apologies for the long post and the stupid? question!

Best regards,

Bart Meersman