Part Number: TMS320F2800157
Hi Team,
I have following queries related to Observer in Instaspin Framework for BLDC control:
1. What are the tolerances for observer in Instaspin Framework?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F2800157
Hi Team,
I have following queries related to Observer in Instaspin Framework for BLDC control:
1. What are the tolerances for observer in Instaspin Framework?
1. What are the tolerances for observer in Instaspin Framework?
What do you mean the tolerances? The resolution of the estimated angle and speed are related to the current and voltage signals, motor electrical parameters like Rs, Ls and Flux. The better signals and the precise motor parameters will improve the performance of the motor control with sensorless FOC includes using FAST estimator.
Hi Yanming,
I think I did not explain my query correctly. In Instaspin the solution predicts the Resistance, Inductance and other motor related parameters. If there is any difference in the estimated values and the predicted values, what is the effect of this on the motor working. Also, what is the maximum possible error or tolerance for this prediction?
If there is any difference in the estimated values and the predicted values, what is the effect of this on the motor working.
As mentioned above. It's also related to the current and voltage sensing circuit on your board.
Also, what is the maximum possible error or tolerance for this prediction?
Sorry, we don't have a specific data can be shared with you.