Other Parts Discussed in Thread: AMC1350, , TMS320F28384S
Hello Expert,
I would like to ask if it is possible to directly connect the output of the AMC1350 after setting the ADC of TMS32028384S to 16bit differential mode and Vref=3.0V.
Internal review results:
Output Vcmout of AMC1350 : 1.34V ~ 1.49V ( normal 1.44V )
The Vcm input range in 16bit Differential mode of TMS320F28377S is as shown in the datasheet below.

Question:
1) In this case, is it impossible to connect directly to the AMC1350 and TMS320F28384S?
2) If no, Is there any other way to directly connect AMC1350 and TMS320F28384S while using them in 16BIT Differential mode?
Best Regards,
Michael