This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSSOLARUINVKIT: ADC GPIO pins

Part Number: TMDSSOLARUINVKIT

Hello.

I have your TMDSSOLARUINVKIT and noticed that you are using lots of ADC pins for measuring reference voltage (such as 1_65V_REF, 0_5V_REF, 0_8V_REF, 2_5V_REF). As I need couple ADC for my project I asking is it safe to use them  for other purposes - such as expand the solar microinverter to have more than one PV panel. Asking in another way... are they needed in TMDSSOLARUINVKIT solar microinwerter or can I use them to other than measuring voltage reference purposes?