Part Number: TMS320F28379D
Break at address "0x3ff16a" with no debug information available, or outside of program code.
I am running the led blink example in tms320f28379d, while the leds are blinking in cpu1, I get the error Break at address "0x3ff16a" with no debug information available, or outside of program code in cpu2 what is the reason for this? I make a selection on the cpu1 cpu2 screen before debugging the code, do I need to make another setting?


I select cpu1 from this screen and then the led blink example works, in the same way when I select cpu2 from this screen I get the following warning, although I run it, it does not work, how can I run this led blink example in cpu2