Part Number: TMS320F28062F
Hi,
C2000 ADCs are accompanied with Post Processing Blocks that are capable of zero-crossing detection which can off-load some calculation burden from the CPU. However, I'm not sure about the reliability of the PPB with noisy ADC results and its performance compared to the software detection employed in the SineAnalyzer library. In short, is it better to use the PPB zero-crossing detection instead of SineAnalyzer's?