Part Number: TMS320F280039C
Other Parts Discussed in Thread: SYSCONFIG
Hi team,
Use CCS (12.4.0) SYSCONFIG (1.17.0) to configure the 280039C MCAN peripheral, and after checking Configure Enable Normal Can, it is found that the actual code generation MCAN_CCCR. ASM setting to 1, enter Restriced Mode instead of Normal Can.
So I want to check after Enable Normal Can is checked, is it means to turn on the mode or cancel the mode?


the left is do not check normal mode, the right is check normal mode.

Could you help on this? Thanks!