Part Number: TMS320F280045
Hi.
I'm using the XDS110 DEBUG prob. on our card which contains the 280045.
the Debugger works fin. but when I try to correct the code and run a debug session, I receive the following ERROR.
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.10.0.00080)
I have to unplug my application from the power supply and start the debugger session and only then it works.
????
shai.