Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Hello,
currently i'm using the launch-xl F280049C. In EQEP model i want to check the QEP phase error, but after all configuration and input signal feeding i'm not getting the phase error interrupt.
to configure this error i used QEP_ex5 _speed_derection of motor example which is available in the C2000 sdk
path: C:\ti\c2000\C2000Ware_4_01_00_00\driverlib\f28004x\examples\eqep
in this example i enabled the phase error interrupt along with the unit time out interrupt.
please help me to resolve this issue