Part Number: TIDM-02002
Other Parts Discussed in Thread: C2000WARE
Hello,
There are two problems I am dealing with in this sample code.
- I am trying to use the main.syscfg gui to change some of the system configurations. By default, the code seems to be running on "C28x". However, when I switch to "CLA" instead, the code does not build regardless of which lab I am trying to build.
This is the error
"> Compilation failure
subdir_rules.mk:9: recipe for target 'clllc_hal.obj' failed
"../clllc_hal.c", line 1229: warning #225-D: function "GPIO_setMasterCore" declared implicitly
"../clllc_hal.c", line 1434: warning #225-D: function "MemCfg_setLSRAMMasterSel" declared implicitly
"../clllc_hal.c", line 1434: error #20: identifier "MEMCFG_LSRAMMASTER_CPU_CLA1" is undefined
1 error detected in the compilation of "../clllc_hal.c".
gmake: *** [clllc_hal.obj] Error 1"
- The second issue is related to "clllc_hal.c". The function "GPIO_setMasterCore" is not defined, and it seems that "GPIO_setControllerCore" is the right one to use.
I am using CCS V12, and C2000Ware_DigitalPower_SDK_4.04.00.00
Thanks,
MK