Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSCNCD28P65X
Hi,
I have customers using TMS320F28388D, now some questions, please help to answer.
1. The customer uses F28388+ DP83826, which is connected through the MII port. Now it is not clear on the hardware pin connection. It is necessary to use the 28 and 29 pins of DP83826, but there is no corresponding pin connected with the 28 and 29 pins in the actual F28388?
Do you have detailed reference documentation?
Many thanks~