Part Number: TMS320F2800137
Other Parts Discussed in Thread: LAUNCHXL-F2800137
Hello,
my customer is currently working with the LAUNCHXL-F2800137 and has run into a problem with the SCIA module.
The SCIA module is initialized and sending data is working correctly.
For reading data, they want to wait for a break event and therefore use the SCI_INT_RXRDY_BRKDT interrupt. The interrupt is also working correctly.
The problem occurs if a SW reset is issued. After that the SCIA module is not waiting for the start bit but starts to fill up the FIFO right away.
This behaviour is shown in the picture below:

Time stamps:
1. Break interrupt
2. SW Reset (sampling starting without the start bit being issued)
3. Next start-bit
4. It can be seen that samping already starts at 2. since there is a framing error in the byte being sent
If a while loop is added to the break interrupt that is waiting for the start bit it is working, however this is not a real solution.
Is there anything else to consider for working correctly with the SCIA module?
Best regards
Manuel