Part Number: TMS320F28388D
Other Parts Discussed in Thread: SYSCONFIG
Hi,
we have the 28388D processor where the system clock and PWM are running at 200Mhz. It appears that the CLB is also running at 200Mhz, but according to the documentation it should only run at 100 or 150Mhz.
We think this is leading to BissC errors.
1. Is there a way to change the CLB clock to run slower and not be reliant on the system clock or PWM?
2. If the CLB clock is running at 200Mhz, I set the pipeline value in the register but no effect. Could this be causing BissC errors.
We were provide the BissC sysconfig file which I was able to load into our project and build it. This seems to have helped but not completely stopped the BissC errors
Any other suggestions would be helpful.
Dorion