Part Number: TMS320F2800157-Q1
Other Parts Discussed in Thread: ADS131M03-Q1, C2000WARE
what frequencies are available for to supply a clock for an ADC
we would like to clock the ADS131M03-Q1 as fast as possible using the TMS320F2800156-Q1
From what I can tell, the ADC has a maximum external clock source of 8.4MHz
The XCLKOUT pin is used to bring out the clock from the MCU and with an MCU system clock of 100MHz.
I was told that the 157 w/ clock of 120MHz had "base frequencies" of 20, 120, and 140 which could be divided down using XCLKOUTDIV by a value of 1, 2, 4, or 8
I dont know if that is 100% accurate and if so I dont know what the 156 base frequencies are that can be divided down.