This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: DCSM RAM/FLASH STATUS

Part Number: TMS320F2800137

1. Based on TRM of DCSM section Table5-1, is the ram ownership and accessiblibity unsecue if both Z1/Z2 grambram bit is configured to 2'b11 and Z1/2 CSM passowds are not pogrammed?

2. Does this configuration has any significance in my application? I think it increase my configuration difficulty.

  • Hello,

    If you have not programmed any CSM passwords, the values of GRABRAMx/GRABSECTx are not relevant. However if either of the zone's passwords are programmed and that zone becomes locked, the corresponding memory region will become inaccessible. If you want a memory region to be unsecure but still secure other memory regions, the GRABRAM/GRABSECT bits corresponding with the unsecure region should be programmed to b10.

    Let me know if you have any further questions.

    Thank you,

    Luke