Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28388D
Hi,
I need pinout of the HSEC connector.
I have the control card and the mcu, I try to understand pin 1 in HSEC goes to pin # ? in the header
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28388D
Hi,
I need pinout of the HSEC connector.
I have the control card and the mcu, I try to understand pin 1 in HSEC goes to pin # ? in the header
Thanks
I send link for the mcu I have:
https://www.mouser.com/datasheet/2/405/1/spruil8b-1951497.pdf
I need pinout for him.
thanks
This is in C2000Ware. https://www.ti.com/tool/C2000WARE
After install the pinout is described here: "C:\ti\c2000\C2000Ware_5_00_00_00\boards\controlCARDs\TMDSCNCD28388D\Rev.B\TMDSCNCD2838x_RevB_180cCARD_pinout.pdf"
The layout can be seen in the parent directory. Please note that the HSEC's pin 1 is not the same as the connectors pin 1.
if you are looking for the spacing to create your own baseboard this may help you https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/659795/tmdscncd28379d-control-card-dimenstions?ReplyFilter=Answers&ReplySortBy=Answers&ReplySortOrder=Descending
Regards,
Cody