Part Number: TMS320F2812
Hi,
I am getting below compilation errors when I try to build the code, I get same kind of error for remaining files, not sure how to resolve it.
Building file: "C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/AppMsg.c"
Invoking: C2000 Compiler
"C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/bin/cl2000" -v28 -ml -mt --include_path="C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/pmc" --include_path="/packages/ti/xdais" --include_path="C:/MCS_HVAD/code/PMC_code_trial/include" --include_path="C:/ti/ccs1230/ccs/tools/compiler/ti-cgt-c2000_22.6.0.LTS/include" --advice:performance=all --define=LARGE_MODEL --define=WDOG_ENABLED --define=TARGET_CPU_FLASH --diag_wrap=off --display_error_number --issue_remarks --verbose_diagnostics --quiet --abi=coffabi -k --asm_listing --asm_define=TARGET_FLASH=1 --asm_define=PLL_SETTING=8 --asm_define=FLASHWAIT=1028 --output_all_syms --asm_directory="C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/Release_Flash" --preproc_with_compile --preproc_dependency="AppMsg.d_raw" --obj_directory="C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/pmc/../Release_Flash" "C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/AppMsg.c"
remark #24038-D: --output_all_syms is deprecated and will be removed in a subsequent release. This is now the default behavior of the compiler.
>> Compilation failure
subdir_rules.mk:9: recipe for target 'C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/Release_Flash/AppMsg.obj' failed
Could Not Find C:\MCS_HVAD\code\PMC_code_trial\SE-0000-28-5 Rev 004-a Source\pmc.hex
"C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/AppMsg.c", line 29: fatal error #1965: cannot open source file "std.h"
#include <std.h>
^
1 catastrophic error detected in the compilation of "C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/AppMsg.c".
Compilation terminated.
gmake[1]: *** [C:/MCS_HVAD/code/PMC_code_trial/SE-0000-28-5 Rev 004-a Source/Release_Flash/AppMsg.obj] Error 1
gmake[1]: *** Waiting for unfinished jobs....