Good afternoon.
There are two pulse signals at the PWM (DC) input. And I need to get the clock signal on the base timer only when they match.
Is it possible to set up a digital comparator so that it works like a logical "AND" for two pulse signals?
For example.
When two pulses arrive at the same time, the digital comparator generates a sync pulse for the base timer.
If the pulses diverge in duration, then the digital comparator did not generate anything.