Hi
When debugging the device in Code Composer Studio, I cannot get the device to flash past sector 7 (0x.
I have updated the .cml file to include sector 8 - see Image 1 attached

When editing the debug configuration settings, only 8 sectors, which is half of the flash memory, is shown. This makes me think that the debugger is not aware of the rest of the flash. See Image 2 attached.

Any suggestions on how I can remedy this would be appreciated.
Regards,
Ezra