This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: Max possible CAN Bus speed using internal oscillator

Part Number: TMS320F2800137


Hi,

Can I achieve 1 MBps baud rate on the CAN Bus using the internal OSC on the 2800137 DSP from min to max operating temperature (OSC drift,...)?

Or what is the max baudrate I can do  in CAN using internal OSC from min to max temperature?

Thanks,

Arnaud

  • Hi Arnaud,

    Thanks for your question.

    Can I achieve 1 MBps baud rate on the CAN Bus using the internal OSC on the 2800137 DSP from min to max operating temperature (OSC drift,...)?

    We cannot support CAN bus with internal OSC, due to the 0.5% accuracy requirement of CAN bus and minimum 1% INTOSC accuracy.

    Regards,

    Vince