Other Parts Discussed in Thread: C2000WARE, TIDA-010054, TMS320F28377D
Hi TI,
I want to implement the close loop control for my system by using TMS320F28379D MCU.
I am using the example code(C2000Ware_DigitalPower_SDK 4.04.00.00/development kit/TIDA-010054-Dual Active Bridge Reference Design/Example Projects/F28004x/dab.h) that was in the resource explorer.
i have shared the code with you for your reference.
Please suggest any probable way to resolve this issue.
.
//#############################################################################
//
// FILE: dab.c
//
// TITLE: This is the solution file.
//
//#############################################################################
// $TI Release: TIDA_010054 v1.00.02.00 $
// $Release Date: Thu Jun 29 23:37:54 CDT 2023 $
// $Copyright:
// Copyright (C) 2023 Texas Instruments Incorporated - http://www.ti.com/
//
// ALL RIGHTS RESERVED
// $
//#############################################################################
//*****************************************************************************
// the includes
//
//*****************************************************************************
#include "dab.h"
//
//--- System Related Globals ---
// Put the variables that are specific to control in the below section
// For example SFRA cannot run on CLA hence it must not be placed
// in the below section, the control verification using SFRA can only
// be carried out on the C28x
// Control Variables
//
#pragma SET_DATA_SECTION("controlVariables")
DAB_buildLevel_enum DAB_buildLevel;
DAB_tripFlag_enum DAB_tripFlag;
DAB_pwmSwState_enum DAB_pwmSwStateActive, DAB_pwmSwState;
DAB_powerFlowState_enum DAB_powerFlowStateActive, DAB_powerFlowState;
DAB_GI DAB_gi;
float32_t DAB_giOut;
float32_t DAB_giError;
float32_t DAB_giPartialComputedValue;
DAB_GV DAB_gv;
float32_t DAB_gvOut;
float32_t DAB_gvError;
float32_t DAB_gvPartialComputedValue;
//
// Flags for clearing trips and closing the loop
//
#pragma RETAIN (DAB_closeGiLoop)
int32_t DAB_closeGiLoop;
#pragma RETAIN (DAB_closeGvLoop)
int32_t DAB_closeGvLoop;
#pragma RETAIN (DAB_clearTrip)
int32_t DAB_clearTrip;
//
// The below variable can be used by the user to enter value through
// the watch window and hence must be volatile
//
#pragma RETAIN (DAB_pwmFrequencyRef_Hz)
float32_t DAB_pwmFrequencyRef_Hz;
#pragma RETAIN (DAB_pwmFrequency_Hz)
float32_t DAB_pwmFrequency_Hz;
#pragma RETAIN (DAB_pwmFrequencyPrev_Hz)
float32_t DAB_pwmFrequencyPrev_Hz;
#pragma RETAIN (DAB_pwmPeriodRef_pu)
float32_t DAB_pwmPeriodRef_pu;
float32_t DAB_pwmPeriod_pu;
float32_t DAB_pwmPeriodMin_pu;
float32_t DAB_pwmPeriodMax_pu;
float32_t DAB_pwmPeriodMax_ticks;
uint32_t DAB_pwmPeriod_ticks;
//
// 1- Primary Side
//
float32_t DAB_iPrimSensed_Amps;
float32_t DAB_iPrimSensed_pu;
float32_t DAB_iPrimSensedOffset_pu;
float32_t DAB_iPrimSensedCalIntercept_pu;
float32_t DAB_iPrimSensedCalXvariable_pu;
EMAVG DAB_iPrimSensedAvg_pu;
float32_t DAB_iPrimTankSensed_Amps;
float32_t DAB_iPrimTankSensed_pu;
float32_t DAB_iPrimTankSensedOffset_pu;
float32_t DAB_iPrimTankSensedCalIntercept_pu;
float32_t DAB_iPrimTankSensedCalXvariable_pu;
EMAVG DAB_iPrimTankSensedAvg_pu;
float32_t DAB_vPrimSensed_Volts;
float32_t DAB_vPrimSensed_pu;
float32_t DAB_vPrimSensedOffset_pu;
float32_t DAB_vPrimSensedCalXvariable_pu;
float32_t DAB_vPrimRef_Volts;
#pragma RETAIN (DAB_pwmDutyPrimRef_pu)
float32_t DAB_pwmDutyPrimRef_pu;
float32_t DAB_pwmDutyPrim_pu;
uint32_t DAB_pwmDutyAPrim_ticks;
uint32_t DAB_pwmDutyBPrim_ticks;
#pragma RETAIN (DAB_pwmDeadBandREDPrimRef_ns)
float32_t DAB_pwmDeadBandREDPrimRef_ns;
uint32_t DAB_pwmDeadBandREDPrim_ticks;
#pragma RETAIN (DAB_pwmDeadBandFEDPrimRef_ns)
float32_t DAB_pwmDeadBandFEDPrimRef_ns;
uint32_t DAB_pwmDeadBandFEDPrim_ticks;
#pragma RETAIN (DAB_pwmPhaseShiftPrimSecRef_pu)
float32_t DAB_pwmPhaseShiftPrimSecRef_pu;
#pragma RETAIN (DAB_pwmPhaseShiftPrimSec_pu)
float32_t DAB_pwmPhaseShiftPrimSec_pu;
float32_t DAB_pwmPhaseShiftPrimSec_ns;
#pragma RETAIN (DAB_pwmPhaseShiftPrimSec_ticks)
int32_t DAB_pwmPhaseShiftPrimSec_ticks;
#pragma RETAIN (DAB_pwmPhaseShiftPrimSec_HiResticks)
uint16_t DAB_pwmPhaseShiftPrimSec_HiResticks;
int16_t DAB_pwmPhaseShiftPrimSec_countDirection;
//
// 2-Secondary side (Battery)
//
float32_t DAB_iSecSensed_Amps;
float32_t DAB_iSecSensed_pu;
float32_t DAB_iSecSensedOffset_pu;
float32_t DAB_iSecSensedCalIntercept_pu;
float32_t DAB_iSecSensedCalXvariable_pu;
EMAVG DAB_iSecSensedAvg_pu;
#pragma RETAIN (DAB_iSecRef_Amps)
float32_t DAB_iSecRef_Amps;
float32_t DAB_iSecRef_pu;
float32_t DAB_iSecRefSlewed_pu;
float32_t DAB_vSecSensed_Volts;
float32_t DAB_vSecSensed_pu;
float32_t DAB_vSecSensedOffset_pu;
float32_t DAB_vSecSensedCalXvariable_pu;
float32_t DAB_vSecRef_Volts;
float32_t DAB_vSecRef_pu;
float32_t DAB_vSecRefSlewed_pu;
float32_t DAB_iSecTankSensed_Amps;
float32_t DAB_iSecTankSensed_pu;
float32_t DAB_iSecTankSensedOffset_pu;
float32_t DAB_iSecTankSensedCalIntercept_pu;
float32_t DAB_iSecTankSensedCalXvariable_pu;
EMAVG DAB_iSecTankSensedAvg_pu;
#pragma RETAIN (DAB_pwmDutySecRef_pu)
float32_t DAB_pwmDutySecRef_pu;
float32_t DAB_pwmDutySec_pu;
uint32_t DAB_pwmDutyASec_ticks;
uint32_t DAB_pwmDutyBSec_ticks;
#pragma RETAIN (DAB_pwmDeadBandREDSecRef_ns)
float32_t DAB_pwmDeadBandREDSecRef_ns;
uint32_t DAB_pwmDeadBandREDSec_ticks;
#pragma RETAIN (DAB_pwmDeadBandFEDSecRef_ns)
float32_t DAB_pwmDeadBandFEDSecRef_ns;
uint32_t DAB_pwmDeadBandFEDSec_ticks;
#pragma RETAIN (DAB_phaseSyncPrimToSecCountDirection)
uint16_t DAB_phaseSyncPrimToSecCountDirection;
#pragma SET_DATA_SECTION()
//
// datalogger
//
DLOG_4CH DAB_dLog1;
float32_t DAB_dBuff1[100];
float32_t DAB_dBuff2[100];
float32_t DAB_dBuff3[100];
float32_t DAB_dBuff4[100];
float32_t DAB_dVal1;
float32_t DAB_dVal2;
float32_t DAB_dVal3;
float32_t DAB_dVal4;
float32_t DAB_dlogTrigger;
//
//--- SFRA Related Variables ---
//
#if DAB_SFRA_TYPE != DAB_SFRA_DISABLED
float32_t plantMagVect[SFRA_FREQ_LENGTH];
float32_t plantPhaseVect[SFRA_FREQ_LENGTH];
float32_t olMagVect[SFRA_FREQ_LENGTH];
float32_t olPhaseVect[SFRA_FREQ_LENGTH];
float32_t freqVect[SFRA_FREQ_LENGTH];
#endif
SFRA_F32 sfra1;
//
//TODO setupSFRA
//
#if DAB_SFRA_TYPE != DAB_SFRA_DISABLED
void DAB_setupSFRA(void)
{
SFRA_F32_reset(&sfra1);
SFRA_F32_config(&sfra1,
SFRA_ISR_FREQ,
SFRA_AMPLITUDE,
SFRA_FREQ_LENGTH,
SFRA_FREQ_START,
SFRA_FREQ_STEP_MULTIPLY,
plantMagVect,
plantPhaseVect,
olMagVect,
olPhaseVect,
NULL,
NULL,
freqVect,
1);
SFRA_F32_resetFreqRespArray(&sfra1);
SFRA_F32_initFreqArrayWithLogSteps(&sfra1,
SFRA_FREQ_START,
SFRA_FREQ_STEP_MULTIPLY);
//
//configures the SCI channel for communication with SFRA host GUI
//to change SCI channel change #defines in the settings.h file
//the GUI also changes a LED status, this can also be changed with #define
//in the file pointed to above
//
SFRA_GUI_config(DAB_SFRA_GUI_SCI_BASE,
DAB_SCI_VBUS_CLK,
DAB_SFRA_GUI_SCI_BAUDRATE,
DAB_SFRA_GUI_SCIRX_GPIO,
DAB_SFRA_GUI_SCIRX_GPIO_PIN_CONFIG,
DAB_SFRA_GUI_SCITX_GPIO,
DAB_SFRA_GUI_SCITX_GPIO_PIN_CONFIG,
DAB_SFRA_GUI_LED_INDICATOR,
DAB_SFRA_GUI_LED_GPIO,
DAB_SFRA_GUI_LED_GPIO_PIN_CONFIG,
&sfra1,
1);
}
#endif
void DAB_initGlobalVariables(void)
{
#if DAB_LAB == 5
DAB_powerFlowStateActive.powerFlowState = powerFlow_BatteryDischarging;
DAB_powerFlowState.powerFlowState = powerFlow_BatteryDischarging;
#else
DAB_powerFlowStateActive.powerFlowState = powerFlow_BatteryCharging;
DAB_powerFlowState.powerFlowState = powerFlow_BatteryCharging;
#endif
//Compensator parameters for voltage loop
DCL_resetDF22(&DAB_gv);
DAB_gv.a1 = DAB_GV_2P2Z_A1;
DAB_gv.a2 = DAB_GV_2P2Z_A2;
DAB_gv.b0 = DAB_GV_2P2Z_B0;
DAB_gv.b1 = DAB_GV_2P2Z_B1;
DAB_gv.b2 = DAB_GV_2P2Z_B2;
//Compensator parameters for current loop
DCL_resetPI(&DAB_gi);
DAB_gi.Ki = DAB_GI_KI;
DAB_gi.Kp = DAB_GI_KP;
DAB_gi.Umax = DAB_GI_UMAX;
DAB_gi.Umin = DAB_GI_UMIN;
DAB_gi.Imax = DAB_GI_IMAX;
DAB_gi.Imin = DAB_GI_IMIN;
DLOG_4CH_reset(&DAB_dLog1);
DLOG_4CH_config(&DAB_dLog1,
&DAB_dVal1, &DAB_dVal2, &DAB_dVal3, &DAB_dVal4,
DAB_dBuff1, DAB_dBuff2, DAB_dBuff3, DAB_dBuff4,
100, 0.5, 1);
DAB_dlogTrigger = 0;
// Unused functions
EMAVG_reset(&DAB_iSecSensedAvg_pu);
EMAVG_config(&DAB_iSecSensedAvg_pu, 0.01);
EMAVG_reset(&DAB_iPrimSensedAvg_pu);
EMAVG_config(&DAB_iPrimSensedAvg_pu, 0.01);
EMAVG_reset(&DAB_iPrimTankSensedAvg_pu);
EMAVG_config(&DAB_iPrimTankSensedAvg_pu, 0.01);
//
// Gui Variables
//
DAB_iPrimSensed_Amps = 0.0f;
DAB_vPrimSensed_Volts = 0.0f;
DAB_iSecSensed_Amps = 0.0f;
DAB_vSecSensed_Volts = 0.0f;
DAB_vSecRef_Volts = DAB_VSEC_NOMINAL;
DAB_vSecRef_pu = DAB_VSEC_NOMINAL / DAB_VSEC_OPTIMAL_RANGE;
DAB_vSecRefSlewed_pu = 0.0f;
DAB_iSecRef_Amps = DAB_ISEC_NOMINAL;
DAB_pwmPeriod_pu = (DAB_MIN_PWM_SWITCHING_FREQUENCY_HZ /
DAB_NOMINAL_PWM_SWITCHING_FREQUENCY_HZ);
DAB_pwmPeriodRef_pu = DAB_pwmPeriod_pu;
DAB_pwmPeriodMin_pu = (DAB_MIN_PWM_SWITCHING_FREQUENCY_HZ /
DAB_MAX_PWM_SWITCHING_FREQUENCY_HZ);
DAB_pwmPeriodMax_ticks = DAB_PWMSYSCLOCK_FREQ_HZ /
DAB_MIN_PWM_SWITCHING_FREQUENCY_HZ;
DAB_pwmFrequencyRef_Hz = DAB_NOMINAL_PWM_SWITCHING_FREQUENCY_HZ;
DAB_pwmFrequency_Hz = DAB_NOMINAL_PWM_SWITCHING_FREQUENCY_HZ;
DAB_pwmFrequencyPrev_Hz = DAB_pwmFrequency_Hz - 1.0f;
DAB_pwmPhaseShiftPrimSec_pu = 0.032f;
DAB_pwmPhaseShiftPrimSecRef_pu = 0.032f;
DAB_pwmPhaseShiftPrimSec_ns = 0.0f;
DAB_pwmDeadBandREDPrimRef_ns = DAB_PRIM_PWM_DEADBAND_RED_NS;
DAB_pwmDeadBandFEDPrimRef_ns = DAB_PRIM_PWM_DEADBAND_FED_NS;
DAB_pwmDeadBandREDSecRef_ns=DAB_SEC_PWM_DEADBAND_RED_NS;
DAB_pwmDeadBandFEDSecRef_ns=DAB_SEC_PWM_DEADBAND_FED_NS;
DAB_iPrimSensed_pu = 0.0f;
DAB_iPrimTankSensed_pu = 0.0f;
DAB_iPrimSensedOffset_pu = 0.5f;
DAB_iPrimTankSensedOffset_pu = 0.5f;
DAB_vPrimSensed_pu = 0.0f;
DAB_vPrimSensedOffset_pu = 0.0f;
DAB_iSecSensed_pu = 0.0f;
DAB_iSecSensedOffset_pu = 0.5f;
DAB_vSecSensed_pu = 0.0f;
DAB_vSecSensedOffset_pu = 0.0f;
DAB_vPrimSensedCalXvariable_pu = 1.024f;
DAB_vSecSensedCalXvariable_pu = 1.01f;
if(DAB_powerFlowState.powerFlowState == powerFlow_BatteryCharging)
{
DAB_pwmDutyPrim_pu = 0.5f;
DAB_pwmDutyPrimRef_pu = 0.5f;
DAB_pwmDutySec_pu = 0.5f;
DAB_pwmDutySecRef_pu = 0.5f;
}
else if(DAB_powerFlowState.powerFlowState == powerFlow_BatteryDischarging)
{
DAB_pwmDutyPrim_pu = 0.5f;
DAB_pwmDutyPrimRef_pu = 0.5f;
DAB_pwmDutySec_pu = 0.5f;
DAB_pwmDutySecRef_pu = 0.5f;
}
DAB_iSecSensedCalIntercept_pu = 0.0f;
DAB_iSecSensedCalXvariable_pu = 1.0f;
DAB_iPrimSensedCalIntercept_pu = 0.0f;
DAB_iPrimSensedCalXvariable_pu = 1.0f;
DAB_iPrimTankSensedCalIntercept_pu = 0.0f;
DAB_iPrimTankSensedCalXvariable_pu = 1.0f;
DAB_pwmSwState.pwmSwState = pwmSwState_singlePhaseShiftControl;
DAB_pwmSwStateActive.pwmSwState = pwmSwState_singlePhaseShiftControl;
DAB_tripFlag.tripFlag = noTrip;
DAB_vPrimRef_Volts = 400.0f;
DAB_closeGiLoop = 0;
DAB_closeGvLoop = 0;
DAB_clearTrip = 0;
}
//
//TODO updateBoardStatus()
void DAB_updateBoardStatus(void)
{
int16_t tripStatusRead;
tripStatusRead = DAB_HAL_readTripFlags();
if(DAB_tripFlag.tripFlag == noTrip)
{
if(tripStatusRead == (int16_t) primOverCurrentTrip)
{
DAB_tripFlag.tripFlag = primOverCurrentTrip;
}
else if(tripStatusRead == (int16_t) secOverCurrentTrip)
{
DAB_tripFlag.tripFlag = secOverCurrentTrip;
}
else if(tripStatusRead == (int16_t) primTankOverCurrentTrip)
{
DAB_tripFlag.tripFlag = primTankOverCurrentTrip;
}
else if(tripStatusRead == (int16_t) secOverVoltageTrip)
{
DAB_tripFlag.tripFlag = secOverVoltageTrip;
}
else
{
DAB_tripFlag.tripFlag = noTrip;
}
}
}
void DAB_runSFRABackGroundTasks(void)
{
//
// new_injection_amplitude=sfra1.freqVect[sfra1.freqIndex]
// SFRA_F32_updateInjectionAmplitude(&sfra1,new_injection_amplitude);
//
SFRA_F32_runBackgroundTask(&sfra1);
SFRA_GUI_runSerialHostComms(&sfra1);
}
void DAB_setBuildLevelIndicatorVariable(void)
{
#if DAB_INCR_BUILD == 1
#if DAB_SEC_CONNECTED_IN_BATTERY_EMULATION_MODE == 0
#if DAB_CONTROL_RUNNING_ON == CLA_CORE
DAB_buildLevel.buildLevel = openLoopCheck_CLA;
#else
DAB_buildLevel.buildLevel = openLoopCheck;
#endif
#else
DAB_buildLevel.buildLevel = undefinedState;
#endif
#elif DAB_INCR_BUILD == 2
#if DAB_SFRA_TYPE == DAB_SFRA_VOLTAGE
#if DAB_SEC_CONNECTED_IN_BATTERY_EMULATION_MODE == 0
#if DAB_CONTROL_RUNNING_ON == CLA_CORE
DAB_buildLevel.buildLevel = closedLoopCheck_Voltage_CLA;
#else
DAB_buildLevel.buildLevel = closedLoopCheck_Voltage;
#endif
#else
DAB_buildLevel.buildLevel = undefinedState;
#endif
#elif DAB_SFRA_TYPE == DAB_SFRA_CURRENT
#if DAB_SEC_CONNECTED_IN_BATTERY_EMULATION_MODE == 0
#if DAB_CONTROL_RUNNING_ON == CLA_CORE
DAB_buildLevel.buildLevel = closedLoopCheck_Current_CLA;
#else
DAB_buildLevel.buildLevel = closedLoopCheck_Current;
#endif
#else
#if DAB_CONTROL_RUNNING_ON == CLA_CORE
DAB_buildLevel.buildLevel =
closedLoopCheck_Current_BatteryMode_CLA;
#else
DAB_buildLevel.buildLevel =
closedLoopCheck_Current_BatteryMode_CLA;
#endif
#endif
#endif
#endif
}
//
// No more.
//