Part Number: TMS320F28388D
Hello C2000 gurus,
The datasheet is a bit unclear on allowable voltage on the VREFHI pins to achieve specified ADC/DAC performance parameters. I have always believed that the VREFHI pin can be driven by a 3.3V ref if the VDDA was also 3.3V. However, the highlighted part from the datasheet below suggests that VREFHI must be below VDDA. Is this correct? Should this instead say VREFHI pin must be at or below VDDA? If VREFHI must be below VDDA then by how much should it be below VDDA? Is the max VREFHI reference limited to 3V when VDDA is 3.3V, in order to achieve specified performance parameters?
Thanks,
Hrishi