Part Number: TMS320F280039
Hello,
I have a problem with the SCI Lab example. The Lab doens't work, it stops in the for loop here
if((rxStatus & SCI_RXSTATUS_ERROR) != 0)
{
//
//If Execution stops here there is some error
//Analyze SCI_getRxStatus() API return value
//
ESTOP0;
The rxStatus is 0.
I also try the solution for this lab and here the program fails at the device.c
void __error__(const char *filename, uint32_t line)
{
//
// An ASSERT condition was evaluated as false. You can use the filename and
// line parameters to determine what went wrong.
//
ESTOP0;
}
I try to find and open this file, but it doesn't exist.
In the terminal I get no output and can also make no input.
I also try the program at an other computer and with an other microcontrollerboard but the problems are the same.
Also changing the position of S1 and S1:A doesn't help.
Currently I don't have the dockingstation, only the TMS320F280039 board. Can this be the cause of the problem?
In the description of the Hardware Setup are Jumper Cables listed, but i could not find out which pins to connect.