Part Number: TMS320F280039C
Other Parts Discussed in Thread: TMS320F28388D
Hello everyone,
I am currently working on a project where I have connected a TMS320F280039C to a TMS320F28388D using jumper wires for the CLK, Data 0, and Data 01 lines (for FSI) and have connected both grounds of docking stations to each other directly to provide common ground configuration. I have tested the transmission and found that it works reliably at a frequency of 30MHz. However, when I increase the frequency to above 30MHz, I observe that not all frames are received by the receiver.I want to utilize the highest speed possible (either 50MHz or 60 MHz).
I am wondering if this issue is occurring because I am not using the adapter board, or if there could be any other reasons for this. Has anyone tested the transmission at higher frequencies by connecting the pins as I have done? Could the adapter board be necessary for reliable transmission at frequencies above 30MHz?
Any insights or suggestions would be greatly appreciated.
Thank you!