Part Number: TMS320F28065
Other Parts Discussed in Thread: C2000WARE
Hi experts,
I have a question about Mailbox data reception.
I modify a back2bak demo code(C:\software\c2000ware\C2000Ware_4_03_00_00\device_support\f2806x\examples\c28\ecan_back2back) in order to test the acceptance mask. I set mailbox 30 and mailbox 31 as receiving mailbox, mailbox13 and mailbox15 as transmitting mailbox. The mailbox30 receives the message from mailbox 13. The mailbox31 receives the message from mailbox 15. I didn't modify the InitECana() and InitECanGpio().
This is the code
#define REC_MBOX31_MSGID_ID 0x784UL
#define REC_MBOX31_LOCAL_FILTER 0x0003FFFF
#define REC_MBOX30_MSGID_ID 0x785UL
#define REC_MBOX30_LOCAL_FILTER 0x0003FFFF
#define REC_MBOX_LAM_LAMI 0x80000000UL
#define REC_MBOX_MSGIN_AME 0x40000000UL
#define REC_MBOX30_LAM_REG ((REC_MBOX30_MSGID_ID<<18)&0x1FFFFFFF | REC_MBOX_LAM_LAMI)
#define REC_MBOX30_MSGID_REG ((REC_MBOX30_MSGID_ID<<18)&0x1FFFFFFF | REC_MBOX_MSGIN_AME)
#define REC_MBOX31_LAM_REG ((REC_MBOX31_MSGID_ID<<18)&0x1FFFFFFF | REC_MBOX_LAM_LAMI)
#define REC_MBOX31_MSGID_REG ((REC_MBOX31_MSGID_ID<<18)&0x1FFFFFFF | REC_MBOX_MSGIN_AME)
void main(void)
{
Uint16 j;
Uint16 i;
struct ECAN_REGS ECanaShadow;
InitSysCtrl();
InitECanGpio();
DINT;
InitPieCtrl();
IER = 0x0000;
IFR = 0x0000;
InitPieVectTable();
MessageReceivedCount = 0;
ErrorCount = 0;
PassCount = 0;
InitECana(); // Initialize eCAN-A module
//transmit setting
ECanaMboxes.MBOX13.MSGID.all = REC_MBOX30_MSGID_REG;// 0x9555AAAF;//
ECanaMboxes.MBOX15.MSGID.all = REC_MBOX31_MSGID_REG;// 0x9555AAAF;//
ECanaMboxes.MBOX30.MSGID.all = REC_MBOX30_MSGID_REG;// 0x9555AAAF;//
ECanaMboxes.MBOX31.MSGID.all = REC_MBOX31_MSGID_REG;//0x9555AAAF;//
ECanaRegs.CANMD.all = 0xC0000000;//CHANGE
ECanaMboxes.MBOX13.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX15.MSGCTRL.bit.DLC = 8;
ECanaMboxes.MBOX13.MDL.all = 0x22222222;
ECanaMboxes.MBOX13.MDH.all = 0x22334455;
ECanaMboxes.MBOX15.MDL.all = 0x11111111;
ECanaMboxes.MBOX15.MDH.all = 0x11223344;
ECanaRegs.CANTA.all = 0xFFFFFFFF; // Clear all TAn bits
ECanaRegs.CANRMP.all = 0xFFFFFFFF; // Clear all RMPn bits
ECanaRegs.CANGIF0.all = 0xFFFFFFFF; // Clear all interrupt flag bits
ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
ECanaLAMRegs.LAM30.all = REC_MBOX30_LAM_REG;
ECanaLAMRegs.LAM31.all = REC_MBOX31_LAM_REG;
ECanaRegs.CANOPC.all = 0xC0000000; //change
//
EALLOW;
ECanaRegs.CANGIM.all = 0x00000000;
ECanaRegs.CANMIM.all = 0xFFFFFFFF;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.STM = 1; // Configure CAN for self-test mode
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
EDIS;
ECanaRegs.CANMD.all = 0xC0000000;
ECanaRegs.CANME.all = 0xC000A000;
//
// Begin transmitting
//
for(;;)
{
//
// Set TRS for all transmit mailboxes
//
ECanaRegs.CANTRS.all = 0x0000A000;
while(ECanaRegs.CANTA.all != 0x0000A000 )
{
}
ECanaRegs.CANTA.all = 0x0000A000;
j=30;
mailbox_read(j);
}
}
void
InitECanaGpio(void)
{
EALLOW;
//
// Enable internal pull-up for the selected CAN pins
// Pull-ups can be enabled or disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pull-up for GPIO30 (CANRXA)
GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pull-up for GPIO31 (CANTXA)
//
// Set qualification for selected CAN pins to asynch only
// Inputs are synchronized to SYSCLKOUT by default.
// This will select asynch (no qualification) for the selected pins.
//
GpioCtrlRegs.GPAQSEL2.bit.GPIO30 = 3; // Asynch qual for GPIO30 (CANRXA)
//
// Configure eCAN-A pins using GPIO regs
// This specifies which of the possible GPIO pins will be eCAN functional
// pins.
//
//
// Configure GPIO30 for CANRXA operation
//
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1;
//
// Configure GPIO31 for CANTXA operation
//
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1;
EDIS;
}
#endif
void
InitECana(void)
{
//
// Create a shadow register structure for the CAN control registers.
// This is needed, since only 32-bit access is allowed to these registers.
// 16-bit access to these registers could potentially corrupt the register
// contents or return false data.
//
struct ECAN_REGS ECanaShadow;
//
// Setup variables to initialize mailboxes to zero
//
int16 mboxCount;
volatile struct MBOX *Mailbox = (void *) 0x6100;
EALLOW; // EALLOW enables access to protected bits
//
// Configure eCAN RX and TX pins for CAN operation using eCAN regs
//
ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
ECanaShadow.CANTIOC.bit.TXFUNC = 1;
ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;
ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
ECanaShadow.CANRIOC.bit.RXFUNC = 1;
ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;
//
// Configure eCAN for HECC mode - (reqd to access mailboxes 16 thru 31)
// HECC mode also enables time-stamping feature
//
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.SCB = 1;
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
//
// Initialize all registers of the mailboxes to zero
// Some bits of MSGCTRL register come up in an unknown state.
// For proper operation, all bits (including reserved bits) of MSGCTRL must
// be initialized to zero
//
for(mboxCount=0; mboxCount<32; mboxCount++)
{
Mailbox->MSGID.all = 0;
Mailbox->MSGCTRL.all = 0;
Mailbox->MDH.all = 0;
Mailbox->MDL.all = 0;
Mailbox = Mailbox + 1;
}
//
// TAn, RMPn, GIFn bits are all zero upon reset and are cleared again
// as a matter of precaution.
//
ECanaRegs.CANTA.all = 0xFFFFFFFF; // Clear all TAn bits
ECanaRegs.CANRMP.all = 0xFFFFFFFF; // Clear all RMPn bits
ECanaRegs.CANGIF0.all = 0xFFFFFFFF; // Clear all interrupt flag bits
ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
//
// Configure bit timing parameters for eCANA
//
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
//
// Wait until the CPU has been granted permission to change the
// configuration registers
//
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set
ECanaShadow.CANBTC.all = 0;
//
// The following block is for 90 MHz SYSCLKOUT.
// (45 MHz CAN module clock Bit rate = 1 Mbps)
// See Note at end of file.
//
ECanaShadow.CANBTC.bit.BRPREG = 2;
ECanaShadow.CANBTC.bit.TSEG1REG = 10;
ECanaShadow.CANBTC.bit.TSEG2REG = 2;
ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
//
// Wait until the CPU no longer has permission to change the
// configuration registers
//
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 0 );// Wait for CCE bit to be cleared
//
// Disable all Mailboxes
//
ECanaRegs.CANME.all = 0; // Required before writing the MSGIDs
EDIS;
}
#endif // endif DSP28_ECANA
If the setting is correct, the mailbox 30 should receive 0x22222222 and 0x22334455. The mailbox 30 should receive 0x11111111 and 0x11223344.
But when I debug, the mailbox30 receives sometimes 0x22222222 and 0x22334455, sometimes 0x11111111 and 0x11223344. It seems that the mailbox30 receives the message of both transmitting mailbox.


But if I comment the code ECanaRegs.CANOPC.all = 0xC0000000;, the problem will not occur anymore.
Could you help me to find out where is wrong?
Besides I want a demo about acceptance mask because I think the setting in this code maybe wrong. I have download in c2000ware_1_00_01_00 which is mentioned in SPRA876B but I can't find the CAN_LAM example in C:\ti\c2000\C2000Ware_1_00_01_00\device_support\f2833x\examples. Could you give me a example about that?
The code is in attachment.
Thanks for your help!!
Best Regards
Kita