This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: CLOSED LOOP IN THE CONTROL CODE AND INVERTER SWITCHING

Part Number: TMS320F28379D
Other Parts Discussed in Thread: TIDA-01606, C2000WARE

Hello:

Can the inverter in the TIDUE531 of rev 2023 be run at 250 kHz? Will the closed-loop feedback code hold up or do we need to modify it substantially?

This is for making a more compact design.

What design features in the Delfino Control Card do we need to pay very close attention to if we have to put its functions - feedback, closed-loop behavior run and JTAG communication for various I/O only functions on board our design?

Will appreciate any help in the matter

r