This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800137: Programming failed

Part Number: TMS320F2800137
Other Parts Discussed in Thread: UNIFLASH, C2000WARE

Hi Team,

There's an issue from the customer need your help:

Using the 2800137 chip, the blank chip can be programmed correctly. After burning to FLASH, the following error message appears after power-on reset, and cannot be burned.

My current solution is to use UniFlash to erase the chip when the card is first powered on.

Want to ask how to solve it?

Error message:

C28xx_CPU1: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
C28xx_CPU1: Trouble Writing Memory Block at 0x5f412 on Page 1 of Length 0x1: (Error -1137 @ 0x5F413) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
C28xx_CPU1: GEL: Error while executing OnTargetConnect(): Target failed to write 0x0005F412@Data
at *((int*) (0x0005F400+0x12))=0x0013 [f2800137.gel:254]
at OnTargetConnect()
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL: Error while executing OnReset(0): identifier not found: pkgType
at (pkgType&(0xFU<<0U)) [f2800137.gel:766]
at Device_Config() [f2800137.gel:210]
at OnReset(0)
C28xx_CPU1: File Loader: Verification failed: Values at address 0x000000@Program do not match Please verify target memory and memory map.
C28xx_CPU1: GEL: File: D:\WORK\gpio_ex2_toggle\CPU1_RAM\gpio_ex2_toggle.out: a data verification error occurred, file load failed.

Thanks & Regards,

Ben