Hi,
I configured ePWM3 to generate a 50Hz output (50% duty), but the result measured is not exactly 50, it is 50.49Hz, is there anyone give me some advices? Thanks a lot!
Felix
unsigned int EPWM3_TIMER_TBPRD = 37500; // Period register - 50Hz, up-down count mode @ 60 MHz/16
void InitEPwm3Example()
{
EPwm3Regs.TBPRD = EPWM3_TIMER_TBPRD; // Set timer period
EPwm3Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm3Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK
EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up-down
EPwm3Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV4; // Clock ratio to SYSCLKOUT
EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV4; // Slow so we can observe on the scope
// Setup compare
EPwm3Regs.CMPA.half.CMPA = EPWM3_TIMER_TBPRD/2;
// Set actions
EPwm3Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM3A on Zero
EPwm3Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm3Regs.AQCTLB.bit.CAU = AQ_CLEAR; // Set PWM3A on Zero
EPwm3Regs.AQCTLB.bit.CAD = AQ_SET;
// Active high complementary PWMs - Setup the deadband
EPwm3Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm3Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm3Regs.DBRED = EPWM3_MIN_DB;
EPwm3Regs.DBFED = EPWM3_MIN_DB;
EPwm3_DB_Direction = DB_UP;
// Interrupt where we will change the deadband
EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event
EPwm3Regs.ETSEL.bit.INTEN = 0; // Enable INT
EPwm3Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 3rd event
}