This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: tms320f28379d CPU 2 flashing problem

Part Number: TMS320F28379D

Hi,

When I am trying load into core 1 Ram and core 2 Ram it is working fine, and it is working fine with core 1 flash also.

But when it comes to core 2 flash I am unable to load the code. I am getting an error window as, it is working in low power mode do you want to exit from it (Yes or No) I did both Yes and no but it is not working. 

Please help me to find out what the issue.

Thanks in Advance.

Thanks & Regards,

K. Aravind,

Sigma Advanced Systems,

9848992750.