Part Number: TMS320F2800157
Other Parts Discussed in Thread: C2000WARE
Hello E2E team,
I am using LUNCHXL-F2800157 for MCAN communication .I am facing problem in loopback tx and rx.
only identifier is being transferred in rx buffer also on attaching the oscilloscope to the can bus the packet is very small than expected
I have attach main.c in code block.
Please help as to what i am doing wrong, i have compared my registers to the given examples for classic tx and loopback
/* Author by : Ram singh
* Date :09/11/2023
* File : main.c
*/
//MCU specific includes
#include "f28x_project.h"
//#include "mcan.h"
//USER INCLUDE FILES
//User define Macros
#define MCAN_MAX_PAYLOAD_BYTES 8U ;
//
// Defines
//
#define MCAN_STD_ID_FILTER_NUM (0U)
#define MCAN_EXT_ID_FILTER_NUM (0U)
#define MCAN_FIFO_0_NUM (0U)
#define MCAN_FIFO_0_ELEM_SIZE (MCAN_ELEM_SIZE_8BYTES)
#define MCAN_FIFO_1_NUM (10U)
#define MCAN_FIFO_1_ELEM_SIZE (MCAN_ELEM_SIZE_8BYTES)
#define MCAN_RX_BUFF_NUM (10U)
#define MCAN_RX_BUFF_ELEM_SIZE (MCAN_ELEM_SIZE_8BYTES)
#define MCAN_TX_BUFF_SIZE (1U)
#define MCAN_TX_BUFF_ELEM_SIZE (MCAN_ELEM_SIZE_8BYTES)
#define MCAN_TX_EVENT_SIZE (10U)
#define MCAN_EXT_ID_AND_MASK (0x1FFFFFFFU)
//#define MCAN_MSG_INT (0x81200)
/**
* \brief Macro for standard Message ID filter.
*/
#define MCANSS_STD_ID_FILTER_SIZE_WORDS (1U)
/**
* \brief Macro for extended Message ID filter.
*/
#define MCANSS_EXT_ID_FILTER_SIZE_WORDS (2U)
//
// Defining Starting Addresses for Message RAM Sections,
// (Calculated from Macros based on User defined configuration above)
//
#define MCAN_STD_ID_FILT_START_ADDR (0x0U)
#define MCAN_EXT_ID_FILT_START_ADDR (MCAN_STD_ID_FILT_START_ADDR + ((MCAN_STD_ID_FILTER_NUM * MCANSS_STD_ID_FILTER_SIZE_WORDS * 4U)))
#define MCAN_FIFO_0_START_ADDR (MCAN_EXT_ID_FILT_START_ADDR + ((MCAN_EXT_ID_FILTER_NUM * MCANSS_EXT_ID_FILTER_SIZE_WORDS * 4U)))
#define MCAN_FIFO_1_START_ADDR (MCAN_FIFO_0_START_ADDR + (MCAN_getMsgObjSize(MCAN_FIFO_0_ELEM_SIZE) * 4U * MCAN_FIFO_0_NUM))
#define MCAN_RX_BUFF_START_ADDR (MCAN_FIFO_1_START_ADDR + (MCAN_getMsgObjSize(MCAN_FIFO_1_ELEM_SIZE) * 4U * MCAN_FIFO_1_NUM))
#define MCAN_TX_BUFF_START_ADDR (MCAN_RX_BUFF_START_ADDR + (MCAN_getMsgObjSize(MCAN_RX_BUFF_ELEM_SIZE) * 4U * MCAN_RX_BUFF_NUM))
#define MCAN_TX_EVENT_START_ADDR (MCAN_TX_BUFF_START_ADDR + (MCAN_getMsgObjSize(MCAN_TX_BUFF_ELEM_SIZE) * 4U * MCAN_TX_BUFF_SIZE))
//User function Prototypes
void MCANInit(void);
int GpioInit(void);
//Global variable
int32_t error = 0;
int32_t loopCnt = 0U;
static uint32_t objSize[8] = {4, 5, 6, 7, 8, 10, 14, 18};
/**
* \brief Enum to represent FIFO/Buffer element Size
*/
typedef enum
{
MCAN_ELEM_SIZE_8BYTES = 0U,
/**< 8 byte data field */
MCAN_ELEM_SIZE_12BYTES = 1U,
/**< 12 byte data field */
MCAN_ELEM_SIZE_16BYTES = 2U,
/**< 16 byte data field */
MCAN_ELEM_SIZE_20BYTES = 3U,
/**< 20 byte data field */
MCAN_ELEM_SIZE_24BYTES = 4U,
/**< 24 byte data field */
MCAN_ELEM_SIZE_32BYTES = 5U,
/**< 32 byte data field */
MCAN_ELEM_SIZE_48BYTES = 6U,
/**< 48 byte data field */
MCAN_ELEM_SIZE_64BYTES = 7U
/**< 64 byte data field */
}MCAN_ElemSize;
//Global struct
typedef struct
{
uint32_t id;
/**< Identifier */
uint32_t rtr;
/**< Remote Transmission Request
* 0 = Transmit data frame
* 1 = Transmit remote frame
*/
uint32_t xtd;
/**< Extended Identifier
* 0 = 11-bit standard identifier
* 1 = 29-bit extended identifier
*/
uint32_t esi;
/**< Error State Indicator
* 0 = ESI bit in CAN FD format depends only on error passive flag
* 1 = ESI bit in CAN FD format transmitted recessive
*/
uint32_t dlc;
/**< Data Length Code
* 0-8 = CAN + CAN FD: transmit frame has 0-8 data bytes
* 9-15 = CAN: transmit frame has 8 data bytes
* 9-15 = CAN FD: transmit frame has 12/16/20/24/32/48/64 data bytes
*/
uint32_t brs;
/**< Bit Rat Switching
* 0 = CAN FD frames transmitted without bit rate switching
* 1 = CAN FD frames transmitted with bit rate switching
*/
uint32_t fdf;
/**< FD Format
* 0 = Frame transmitted in Classic CAN format
* 1 = Frame transmitted in CAN FD format
*/
uint32_t efc;
/**< Event FIFO Control
* 0 = Don’t store Tx events
* 1 = Store Tx events
*/
uint32_t mm;
/**< Message Marker */
uint16_t data[8];
/**< Data bytes.
* Only first dlc number of bytes are valid.
*/
}MCAN_TxBufElement;
typedef struct
{
uint32_t id;
/**< Identifier */
uint32_t rtr;
/**< Remote Transmission Request
* 0 = Received frame is a data frame
* 1 = Received frame is a remote frame
*/
uint32_t xtd;
/**< Extended Identifier
* 0 = 11-bit standard identifier
* 1 = 29-bit extended identifier
*/
uint32_t esi;
/**< Error State Indicator
* 0 = Transmitting node is error active
* 1 = Transmitting node is error passive
*/
uint32_t rxts;
/**< Rx Timestamp */
uint32_t dlc;
/**< Data Length Code
* 0-8 = CAN + CAN FD: received frame has 0-8 data bytes
* 9-15 = CAN: received frame has 8 data bytes
* 9-15 = CAN FD: received frame has 12/16/20/24/32/48/64 data bytes
*/
uint32_t brs;
/**< Bit Rat Switching
* 0 = Frame received without bit rate switching
* 1 = Frame received with bit rate switching
*/
uint32_t fdf;
/**< FD Format
* 0 = Standard frame format
* 1 = CAN FD frame format (new DLC-coding and CRC)
*/
uint32_t fidx;
/**< Filter Index */
uint32_t anmf;
/**< Accepted Non-matching Frame
* 0 = Received frame matching filter index FIDX
* 1 = Received frame did not match any Rx filter element
*/
uint16_t data[8];
/**< Data bytes.
* Only first dlc number of bytes are valid.
*/
}MCAN_RxBufElement;
MCAN_RxBufElement rxMsg;
MCAN_TxBufElement txMsg;
void LoadingTXFIFO(const MCAN_TxBufElement *txMsg)
{
// DATA COPY TO Massage RAM base Address 0X58000
uint32_t *baseAddr;
uint32_t reg_val = 0;
uint16_t adressOffset = 0;
baseAddr = (MCAN_TX_BUFF_START_ADDR + 0x58000U);
//TX element E0
reg_val = ((txMsg->id << 0) | (txMsg->rtr << 29) | (txMsg->xtd << 30)
| (txMsg->esi << 31));
*baseAddr = reg_val;
reg_val = 0;
adressOffset += 4U;
//TX element E1
baseAddr = (baseAddr + adressOffset);
reg_val = ((txMsg->dlc << 16) | (txMsg->brs << 20) | (txMsg->fdf << 21)
| (txMsg->efc << 23) | txMsg->fdf << 24);
*baseAddr = reg_val;
reg_val = 0;
adressOffset += 4U;
//DATA ELEMENT 0
baseAddr = (baseAddr + adressOffset);
reg_val = ((txMsg->data[0] << 0) | (txMsg->data[1] << 8)
| (txMsg->data[2] << 16) | (txMsg->data[3] << 24));
*baseAddr = reg_val;
reg_val = 0;
adressOffset += 4U;
//DATA ELEMENT 1
baseAddr = (baseAddr + adressOffset);
reg_val = ((txMsg->data[4] << 0) | (txMsg->data[5] << 8)
| (txMsg->data[6] << 16) | (txMsg->data[7] << 24));
*baseAddr = reg_val;
reg_val = 0;
}
void CanMassageFrame(MCAN_TxBufElement *txMsg)
{
int i = 0;
volatile uint32_t mode = 0U;
uint32_t dataBytes = 4;
// Initialize message to transmit.
//
txMsg->id = ((uint32_t) (0x111));
txMsg->rtr = 0U;
txMsg->xtd = 0U;
txMsg->esi = 0U;
txMsg->dlc = 8U;
txMsg->brs = 0U;
txMsg->fdf = 0U;
txMsg->efc = 1U;
txMsg->mm = 0xAAU;
// txMsg->data[0] = 0x12;
// txMsg->data[1] = 0x34;
// txMsg->data[2] = 0x56;
// txMsg->data[3] = 0x78;
txMsg->data[i] = 0x1;
for (i = 1; i < dataBytes; i++)
{
txMsg->data[i] = txMsg->data[i - 1] + 1;
}
i = 0;
}
void DataReadFromRxfifo(MCAN_RxBufElement *rxMsg)
{
//Data Read from RX FIFO Address
uint32_t *baseAddr;
uint32_t reg_val = 0;
uint16_t adressOffset = 0;
baseAddr = (MCAN_FIFO_0_START_ADDR + 0x58000U); //0x000002EC;
//RX element E0
reg_val = *baseAddr;
rxMsg->id = reg_val & 0x1FFFFFFF;
rxMsg->rtr = reg_val & 0x20000000;
rxMsg->xtd = reg_val & 0x40000000;
rxMsg->esi = reg_val & 0x80000000;
reg_val = 0;
adressOffset += 4U;
//RX element E1
baseAddr = (baseAddr + adressOffset);
reg_val = *baseAddr;
rxMsg->rxts = reg_val & 0x000000FF;
rxMsg->dlc = reg_val & 0x000F0000;
rxMsg->brs = reg_val & 0x00100000;
rxMsg->fdf = reg_val & 0x00200000;
rxMsg->fidx = reg_val & 0x7F000000;
rxMsg->anmf = reg_val & 0x80000000;
reg_val = 0;
//RX element E1
baseAddr = (baseAddr + adressOffset);
reg_val = *baseAddr;
rxMsg->data[0] = reg_val & 0x000000FF;
rxMsg->data[1] = ((reg_val & 0x0000FF00) >> 8);
rxMsg->data[2] = ((reg_val & 0x00FF0000) >> 16);
rxMsg->data[3] = ((reg_val & 0xFF000000) >> 24);
reg_val = 0;
//RX element E1
baseAddr = (baseAddr + adressOffset);
reg_val = *baseAddr;
rxMsg->data[4] = (reg_val & 0x000000FF);
rxMsg->data[5] = ((reg_val & 0x0000FF00) >> 8);
rxMsg->data[6] = ((reg_val & 0x00FF0000) >> 16);
rxMsg->data[7] = ((reg_val & 0xFF000000) >> 24);
reg_val = 0;
}
void DataReadFromRxbuffer(MCAN_RxBufElement *rxMsg)
{
// DATA Read From Rx Buffer start address
uint32_t *baseAddr;
uint32_t reg_val = 0;
uint16_t adressOffset = 0;
baseAddr = (MCAN_RX_BUFF_START_ADDR + 0x58000U);
//RX element E0
reg_val = *baseAddr;
rxMsg->id = reg_val & 0x1FFFFFFF;
rxMsg->rtr = reg_val & 0x20000000;
rxMsg->xtd = reg_val & 0x40000000;
rxMsg->esi = reg_val & 0x80000000;
reg_val = 0;
adressOffset += 4U;
//RX element E1
baseAddr = (baseAddr + adressOffset);
reg_val = *baseAddr;
rxMsg->rxts = reg_val & 0x000000FF;
rxMsg->dlc = reg_val & 0x000F0000;
rxMsg->brs = reg_val & 0x00100000;
rxMsg->fdf = reg_val & 0x00200000;
rxMsg->fidx = reg_val & 0x7F000000;
rxMsg->anmf = reg_val & 0x80000000;
reg_val = 0;
//RX element E1
baseAddr = (baseAddr + adressOffset);
reg_val = *baseAddr;
rxMsg->data[0] = reg_val & 0x000000FF;
rxMsg->data[1] = ((reg_val & 0x0000FF00) >> 8);
rxMsg->data[2] = ((reg_val & 0x00FF0000) >> 16);
rxMsg->data[3] = ((reg_val & 0xFF000000) >> 24);
reg_val = 0;
//RX element E1
baseAddr = (baseAddr + adressOffset);
reg_val = *baseAddr;
rxMsg->data[4] = (reg_val & 0x000000FF);
rxMsg->data[5] = ((reg_val & 0x0000FF00) >> 8);
rxMsg->data[6] = ((reg_val & 0x00FF0000) >> 16);
rxMsg->data[7] = ((reg_val & 0xFF000000) >> 24);
reg_val = 0;
}
void ReadRXFIFO0(MCAN_RxBufElement *rxMsg)
{
//Data Read from RX FIFO Address
DataReadFromRxfifo(rxMsg);
// DATA Read From Rx Buffer start address
DataReadFromRxbuffer(rxMsg);
}
int main(void)
{
InitSysCtrl();
GpioInit(); // Gpio init
MCANInit(); //CAN init
CanMassageFrame(&txMsg);
LoadingTXFIFO(&txMsg); // DATA COPY TO Massage RAM base Address 0X58000
int i = 0;
uint32_t dataBytes = 8;
// Initialize message to receive
//
rxMsg.id = 0U;
rxMsg.rtr = 0U;
rxMsg.xtd = 0U;
rxMsg.esi = 0U;
rxMsg.rxts = 0U; // Rx Timestamp
rxMsg.dlc = 0U;
rxMsg.brs = 0U;
rxMsg.fdf = 0U;
rxMsg.fidx = 0U; // Filter Index
// (of matching Rx acceptance filter element)
rxMsg.anmf = 0U; // Accepted Non-matching Frame
for(i = 0; i < dataBytes; i++) // Initialize receive buffer to 0
{
rxMsg.data[i] = 0;
}
while (1)
{
// Add request for all transmission.
McanaRegs.MCAN_TXBAR.bit.AR0 = 1;
DELAY_US(10000);
ReadRXFIFO0(&rxMsg);
if(McanaRegs.MCAN_RXF0S.bit.F0F == 1)
{
// while(1)
{
}
}
}
return 0;
}
void MCANInit(void)
{
EALLOW;
McanaRegs.MCAN_CCCR.bit.INIT=1; // MCAN Initialization enable bit. Setting this bit high does not mean that the mcan module is initialized
while(McanaRegs.MCAN_CCCR.bit.INIT==0);
McanaRegs.MCAN_CCCR.bit.CCE=1; // protection bit disable
McanaRegs.MCAN_CCCR.bit.TEST=1;
McanaRegs.MCAN_TEST.bit.LBCK = 1; // Loop Back Mode
McanaRegs.MCAN_CCCR.bit.FDOE=0; // CANFD disable
McanaRegs.MCAN_CCCR.bit.BRSE=0; // Bit rate switch disable
// Bit Nominal bit Rate 1 Mbps as this value is calculated as per DATA sheet
McanaRegs.MCAN_NBTP.bit.NBRP=5; //Nominal Bit Rate Prescaler
McanaRegs.MCAN_NBTP.bit.NTSEG1=12; //Nominal Time Segment Before Sample Point
McanaRegs.MCAN_NBTP.bit.NTSEG2=5; //Nominal Time Segment After Sample Point
McanaRegs.MCAN_NBTP.bit.NSJW=0; //Nominal (Re)Synchronization Jump Width
;
// RX FIFO configuration
McanaRegs.MCAN_RXF0C.bit.F0OM =1; // F0OM = 0: blocking mode enable / F0OM= 1 overwrite mode enable
McanaRegs.MCAN_RXF0C.bit.F0WM =0; // F0WM = 0: water mark interrupt disable / F0WM = 1 to 64 : level for RXFIFO water mark interrupt (IR.RF0W)
McanaRegs.MCAN_RXF0C.bit.F0S =9; // F0S = 0: NO RXFIFO0 / F0S= 1 to 64 RX FIFO Element : TOTAL RX ELEMENT (FOS-1)
McanaRegs.MCAN_RXF0C.bit.F0SA = (MCAN_FIFO_0_START_ADDR>>2); //0x00058006; //MCAN_FIFO_0_START_ADDR ; // START ADDRESS OF RxFIFO RAM : this value should be change
McanaRegs.MCAN_RXESC.bit.F0DS =5; // Rx FIFO 0 Data Field Size
McanaRegs.MCAN_RXBC.bit.RBSA = (MCAN_RX_BUFF_START_ADDR>>2); //0x0005800C;
// TX FIFO configuration
McanaRegs.MCAN_TXBC.bit.TFQM = 0; //TX FIFO MODE (TX FIFO = 0/Queue Mode =1)
McanaRegs.MCAN_TXBC.bit.TBSA = (MCAN_TX_BUFF_START_ADDR>>2); //0x00058000; //TX Buffers Start Address
McanaRegs.MCAN_TXBC.bit.NDTB = 10; //Number of Dedicated Transmit Buffers
McanaRegs.MCAN_TXBC.bit.TFQS = 8; //Number Tx buffer is used as Transmit FIFO/Queue there is waring (NDTB +TFQS!>32)
McanaRegs.MCAN_CCCR.bit.CCE=0; // protection bit disable
McanaRegs.MCAN_CCCR.bit.INIT=0; // Init Mode disable
EDIS;
}
int GpioInit(void)
{
EALLOW;
GpioCtrlRegs.GPALOCK.all = 0; //unlock all GPIO pin
ClkCfgRegs.CLKCFGLOCK1.bit.AUXCLKDIVSEL = 0; //MCAN Clock prescaler enable set to 1
ClkCfgRegs.AUXCLKDIVSEL.bit.MCANCLKDIV = 0; //MCAN Clock prescaler value
//GPIO MUX for MCAN GPIO4 CAN TX and MCAN GPIO5 CANRX
GpioCtrlRegs.GPAGMUX1.bit.GPIO4 = 0;
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 0x3;
GpioCtrlRegs.GPAGMUX1.bit.GPIO5 = 0b01;
GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 0b01;
EDIS;
return 0;
}
uint32_t MCAN_getMsgObjSize(uint32_t elemSize)
{
// ASSERT(elemSize < 8U);
return(objSize[elemSize]);
}
thanks in advance.