Part Number: TMS320F280039
Hi experts,
My customer use the F280039 CAN FD to communicate with the other ARM MCU, with a baud rate of 1M+5M. F280039 sends the data to the ARM neutralizer with a 5ms timer. When the CAN FD cable is unplugged and then reconnected it the F280039 is unable to send or receive data, cannot reconnect automatically, and the ARM neutralizer is still sending frames at 1s intervals. With the DCAN peripheral of the C2000, communication can be restored automatically after the disconnect is reconnected. Could MCAN realize this function and how to realize it? There is also the arbitration domain detection mechanism with DCAN that can be used to identify module nodes with the same address code on the same bus, but it seems that MCAN does not have this function, right?