Part Number: TMS320F28377D
Hi,
I want to run a program in CPU1 (not in CLA1) of the 28377D and I want the maximum amount of RAM to store the program and the data structures. Consequently, I have the following questions:
1) In the 28377D, the LSx, Dx and GSx memories have contiguous addresses. But is it possible to allocate a data section or a software section in [ LS5 + D0 + D1 + GS0] even if these memories have not the same functionalities ?
2) Is it possible to run in CPU1 a software allocated in LSx memory whithout any restriction of the software instruction set (as it is the case for the CLA1).
Thanks for your help.
Best regards.