Hi
I have been using the ezdspf28335 dsp evaluation board for sometime now,for motor control application. Now i intend to use it in a different application (running a simulink motor model ON the DSP).
I have got some weird doubts in trying to move into this application. I guess i'ld get some answers here.
1. Is there a possibility to give DIGITAL INPUTS to the ezdsp board? If so...what is the maximum sampling rate(frequency of the digital signal) it can accept?
2. is there a possibility to extend the On-chip programming flash RAM? Can we use the memory from an external SD-RAM? If so, whats the procedure?
3. Am i moving in the right direction with my application? (is it possible firstly!)
I wonder how i've worked with the DSP with so many weirdo stuff in ma mind!
Expecting some useful answers!