Hi Gurus:
I want to know the impedance before GPIO when no power apply on MCU.
I have application need to connect two C2000 device together, and one use GPIO32 which also can be as boot mode select pin.
To prevent undefined boot behavier, I need to know the state/impedance or is it open-drain or something.
The only thing I know is during power on, all GPIO is high impedance state, but no information about before power on state.
Thanks, best reguards