dear Sir:
Do you have example for "Torque Control"?
I need use TMS28035 to run 3-phase Sensored PMSM Control.
Best Regard
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear Sir:
Do you have example for "Torque Control"?
I need use TMS28035 to run 3-phase Sensored PMSM Control.
Best Regard
Have you checked the examples provided with Control Suite download? Any vector controlled implementation can be potentially used as torque control system by controlling Iq current. Do you only have torque loop? Am curious to know your application.. if possible please share more information on your system and requirements.
dear sir :
thank your answer .
1. yes I Know the Iq value is use for control Torque but how to Calculate the Speed of Torque(Run Continuous and stall) .
in the example Code no Formula to understand. for more Detailed information can't Paste here . please give me your E-mail !!
2. I have two CCS4 error pictures copy from screen that information want send it by E-mail for you.
Best Regard
Sorry, was not able to understand what is meant by "...the speed of torque”... If you are concerned about the response time then the torque loop should take care of your response performance. A typical way to implement is to use PID... Your PID will also take care of stall when properly tuned. I am not sure if you are also looking for a speed loop or not ...anyway, please make sure to draw a system diagram to identify all the required functions for your system.
By the way, your best resource to resolve any CCS or other tool related issue is TI ... please forward your questions to TI hot line.
many thank for Mr. Arefeen.
it look like this (Renesas ) but not same Motor type:
The "Sinusoidal Commutation for BDLC Motors " Shaft Torque Formula include Shaft Angle and current Value.
It can get Motor Torgue value at any speed simply.
I wish the TI employee have this papers to describe Formula of 3-phase Sensored PMSM.
Best Regard
Shaft Torque = Kt [IR Sin(o) + IS Sin(o+120) + IT Sin(o+240)]
where:
o is the electrical angle of the shaft,
Kt is the torque constant of the motor and
IR, IS and IT are the phase currents.
If the phase currents are sinusoidal: IR = I0Sino; IS = I0Sin (+120o); IT = I0Sin (+240o)
this reduces to:
Shaft Torque = 1.5I0*Kt (a constant independent of the shaft angle)