Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH
Hi,
What is the best method of programing code and security settings in production? Optimum would be 'one click' method.
I used UniFlash and tried to do the sequence:
- prorgam code in flash CPU01
- prorgam code in flash CPU02
- prorgam security settings for CPU01 Zone 1
- prorgam security settings for CPU01 Zone 2
- prorgam security settings for CPU02 Zone 1
- prorgam security settings for CPU02 Zone 2
Unfortunatelly after [3] when I was trying to program Zone 2 the error appears:
[ERROR] C28xx_CPU1: Error connecting to the target: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 9.10.0.00080)
Regards,
Piotr Romaniuk