Part Number: TMS320F280037C
Other Parts Discussed in Thread: SYSCONFIG
Hello,
I am interested in configuring our microcontroller as single boot option with flash default so always will be runing in flash no matter the boot pin config pins. However, I am not able to find where the values need to be written. From the technical reference manual in section 4.5.1, it states that the configuration of boot pins is done trhough the DCSM module in Z1 OTP config. When I look at the registers given in the register config approach the struct definition does not mention anything about the boot pin config.
I would like to know which register direction should I change to configure microcontrollers's booting capabilities.
Regards,
David