Part Number: TMS320F2800137
Hi All,
I'm using "sci_ex1_loopback" example of SCI, changing the RX TX pins to relevant on my board and receiving the following terminal messages:
I'm using XDS110 debug probe (which have two connectors, first is 'Debug' and second is 'AUX. FUNCTIONS'), therefore I have two COM ports.
My board JTAG ('Debug') connector is the following:
While pin 17 and 19 is manually connected to UART pins on 'AUX. FUNCTIONS' connector pins 12 and 14 corresponding (17->12 ; 19->14) :
Please advise.