Part Number: TMS320F28335
I am trying to convert the control code for thebTIDA-010210 11-kW, Bidirectional, Three-Phase ANPC Based on GaN Reference Design to be compatible with the F28335 DSP instead of using the F280049C. I have the code where it will flash into the F28335 but nothing appears to actually be running in the debugger. Is this a common error when swapping between microcontrollers? Does anyone have any advice or something I might have missed when making the swap?