Other Parts Discussed in Thread: TMS320F280041C
In Code Composer Studio (v11.1), I moved from the Launchpad (TI LAUNCHXL-F280049C) to the application hardware using an XDS100V2 USD Debug Probe. I went into the target configuration .ccxml and selected the XDS100V2 and the target device (which is the TMS320F280041C). I successfully test the connection using the XDS100V2. I can run code and set breakpoints, inspect parameters, etc. But when I make code changes, build, load, and start debugging again, I am running into JTAG errors. I have seen error code 150 and error -1044. With these errors, I have to power down my whole system and start over in order to debug again. Is there is anything else I need to do to transition from the LauchPad to an XDS100V2?. For example, I see IcePick_C_0 in the Advanced Target Configuration and I see GEL Output statements during download.
Please help me eliminate these errors.