Part Number: TMS320F28386S
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
Hi there,
I am working on an application with CAN (Controller Area Network), and I would like to use the CAN Peripheral from the CM (Communication Manager). I had looked at the example programs of the C2000Ware, but I am using the sysconfig tool (which isn't used in the examples of CM/CAN) to configure the microcontroller. However, to configure the CAN's pins, I need to add a CAN module that adds the CAN_init() function inside the Board_init() function. But when I allocate this CAN Peripheral to CM before calling this function, it's impossible to C28x Init the RAM through the CAN_initRAM() function, causing the software to get stuck in a loop.
Is there any resource to remove this function(CAN_init or myCAN_init) from my board.c source file? Or will I have to make the pinmux of this peripheral by myself without using the sysconfig tool?
Thank you for your guidance,
Ramon Martins.