Part Number: TMS320F280037C
I am working on a 350W charger with an analog design ( hardware part) Previously there was an existing design of a 750W charger digital design which included a lot of programming. 37C micro was used there. I want to reduce the cost by using a low cost microcontroller which does not include a lot of programming. But how to decide which one is suitable
My basic requirements are I need
1) CAN communication- 1 channel
2) SPI channels- 2
ADC pins- 5
DAC pins- 2
GPIO pins- 4
I am stuck at determining how much flash and how much RAM we need for the microcontroller. what is the difference between flah and ram and how much space it occupies? what effects will be there if we choose less memory microcontroller