Part Number: TMS320F280034
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE
We are bringing up the code for a new C2000 custom board design and I thought we would try to use sysconfig for the first time to help with this. We imported the empty_sysconfig_64pm project from C2000Ware under the f28003x examples folder:=-
C:\ti\c2000\C2000Ware_4_03_00_00\driverlib\f28003x\examples
the sysconfig tool runs correctly and we are able to choose the peripheral setup we want and it generates the code we need successfully. However, when I try to compile this code, we have an error with seemingly a redefinition of some of the base addresses of the peripherals. Here is the problem list:-

If I look in more detail at the code generated by sysconfig where the issue is flagged, the problem line seems to be in board.h and is:-
#define EPWM1_BASE EPWM1_BASE
Is there some sort of mulitple definition of what EPWM1_BASE is?
Thanks,
Iain