This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: XDS100v2 on custom board

Part Number: TMS320F28388D

Hi,

we want to implement XDS100v2 on board JTAG Port Debugger on our custom boards.

Reference Schematic can be found on Evaluation Board:

Questions:

1)

Besides JTAG-Port and SCI-Uart Transceiver Lines there are two additional signals with pullup and pulldown and two LED signal lines. Are these lines used and driven by software tools like Code Composer Studio? Which function do they support?

2)

We want to use some more IO Pins on the same FTDI Chip that are not connected either on Port A or B in your XDS100v2 reference design to be used with our own software tools. Is this possible or will software tools like Code Composer Studio drive or configure these pins as well to any specific state....

3)

Is there a possibility (driver description, software API) to develop our own standalone software programming tool? ... waht we need is any library or documentation how to use JTAG Port commands in order to program any hex-file to the device....

Many thanks in advance,

Jeremias