Part Number: TMS320F28379D
Greetings,
I am using CCS 10.4.0.00006 and TI Compiler Version TI v20.2.5.LTS. In the project Properties -> Build -> C2000 Compiler -> Advanced Options -> Language Options, there is a field called “C++ Dialect” with a drop down box which offers, among others, C++ 03 mode and Embedded C++. I have looked in spru514y and can only see a little on each one, main what is not supported in each. Would the compiler produce a difference in size or speed with one or the other?
Thank you,
Ed